Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
List of Accessories Available for PowerLogic A125 Arc Flash Protection Relay

Article available in these languages: Spanish

Issue:

What accessories are available for the PowerLogic A125 arc flash protection relay?

Product:

PowerLogic A125 Arc Flash Protection Relay

Environment:

Low- and medium-voltage switchgear applications using PowerLogic A125 for arc flash protection.

Cause:

Users need to know the compatible accessories for proper installation, maintenance, and system expansion of the PowerLogic A125.

Resolution:

The following accessories are available for PowerLogic A125:

  • Arc Sensors (Point Type):
    • REL52804 – VA1 DA-6 (Cable length 6 m)
    • REL52801 – VA1 DA-20 (Cable length 20 m)
    • REL52806 – VA1 DA-6S (Shielded, 6 m)
    • REL52803 – VA1 DA-20S (Shielded, 20 m)
    • REL52805 – VA1 DA-6S-HF (Halogen-free, 6 m)
    • REL52802 – VA1 DA-20S-HF (Halogen-free, 20 m)
    • REL52839 – VA1 DA-6W (Shielded at sensor end, 6 m)
    • REL52840 – VA1 DA-20W (Shielded at sensor end, 20 m)
  • Arc Sensors (Pipe Type):
    • REL52809 – VA1 EH-6 (6 m)
    • REL52807 – VA1 EH-20 (20 m)
    • REL52810 – VA1 EH-6S (Shielded, 6 m)
    • REL52808 – VA1 EH-20S (Shielded, 20 m)
  • Mounting Accessories:
    • REL52828 – VYX 001 (Surface mounting plate, Z-shaped)
    • REL52829 – VYX 002 (Surface mounting plate, L-shaped)
    • REL52903 – Door mount bracket (For PowerLogic A125 and A3F, IP20)

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: