Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Periodic Testing Recommendations for PowerLogic A125 Arc Flash Protection Relay

Article available in these languages: Spanish

Issue:

How often should the PowerLogic A125 arc flash protection relay be tested, and what methods are recommended?

Product:

PowerLogic A125 Arc Flash Protection Relay

Environment:

Low- and medium-voltage switchgear installations where arc flash protection systems are deployed for personnel and equipment safety.

Cause:

Arc flash protection systems are critical safety components. Over time, environmental conditions, mechanical wear, or wiring changes can affect sensor performance and relay operation. Without periodic testing, there is a risk of undetected faults, delayed tripping, or complete failure during an arc flash event.

Resolution:

The recommendations are:

  • Perform functional testing at least every five (5) years.
  • Testing should include the relay logic, cabling, and arc sensors to ensure the entire protection chain works as intended.
  • Use a secondary injection testing principle for protection stages involving current measurement. This simulates real operating conditions without exposing personnel to actual arc hazards.

Why Testing Matters:

  • Safety Compliance: Many national and industry standards require periodic verification of protection systems.
  • Reliability Assurance: Ensures sensors detect light correctly and trip relays respond within the specified time (as fast as 2 ms for HSO output).
  • Preventive Maintenance: Identifies issues such as dirty sensors, loose connections, or degraded cables before they cause failures.

Practical Tips for Testing:

  • Schedule testing during planned outages to avoid operational disruptions.
  • Document all test results for compliance audits and future reference.
  • After any system modification, sensor replacement, or wiring changes, perform a full functional test immediately.
  • Combine testing with visual inspections (every 3 years) to check for dirt, mechanical damage, or improper sensor positioning.

Additional Considerations:

  • If the system includes multiple A125 units in a selective protection scheme, verify inter-unit communication (Master Trip In/Out signals).
  • Ensure DIP switch settings are correct after maintenance; incorrect settings can compromise protection logic.
  • Test the self-supervision feature by simulating sensor faults to confirm the Service LED and SF output activate properly.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: