Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Configuration Methods for PowerLogic A3 Arc Flash Protection Relay

Article available in these languages: Spanish

Issue:
How can PowerLogic A3 Arc Flash protection be configured for different protection schemes and system requirements?

Product:
PowerLogic A3 Arc Flash Protection Relay

Environment:
Switchgear installations requiring flexible configuration options.

Cause:
Incorrect configuration can lead to nuisance tripping or failure to operate during an arc flash event.

Resolution:
PowerLogic A3 offers three configuration methods:

  1. Rotary Switch & Push Button
    • Quick setup for single devices or small systems.
    • Two rotary switches set Protection Scheme (positions 1–6) and Light Group (positions 1–9).
    • Push button used for Install/Reset and entering Test Mode.
    • Default: Scheme #1, Light Group 1, Current Group 16.
  2. eSetup Easergy Pro Software
    • Requires REL52960 configuration cable.
    • Allows full parameter customization: Protection Scheme, Light Group, Current Group, Output Latch.
    • Supports saving/loading configuration files and advanced diagnostics.
  3. ArcEM Configurator in V321
    • Used when A3 operates as I/O peripheral of V321.
    • Centralized configuration for large systems.
    • Enables mapping of Light Groups (1–12) and Current Groups (13–16) for selective tripping.

Best Practices:

  • Always verify scheme and group settings before commissioning.
  • Use Test Mode to validate sensor wiring and logic without tripping breakers.
  • Change default passwords for cybersecurity.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: