Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where to Find the Selection Guide for L-TRI5 Switch Disconnectors

Article available in these languages: Spanish

Issue:
Users need to locate the selection guide for the L-TRI5 product to choose the correct variant for their application.

Product:
L-TRI5 Indoor Switch Disconnectors (Medium Voltage Distribution up to 36 kV)

Environment:
Indoor medium-voltage switchgear systems requiring reliable and economic switch disconnectors for load switching, ring mains, transformers, cables, and overhead lines.

Cause:
The selection guide contains essential information such as product range, type designation, mounting options, and technical characteristics. Without this guide, users may select incorrect configurations, leading to operational issues or non-compliance with standards.

Resolution:
The Selection Guide for L-TRI5 is located in the next link: HERE

Also is attached to the present article.

Schneider Electric Egypt and North East Africa

Attachment(s)
L-TRI5_PJ_E.pdf [2.79 MB]