Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to online Install a Brand-New M580 CPU in a hot standby system

When installing a brand-new CPU during the production operation of the system,

-do not connect the network cable between the master and standby CPUs.

After the CPU and CRA are all fully operational, connect the network cable to construct the ring network.

-Alternatively, in accordance with the operating procedure outlined in the user manual,

you can first download the program to the brand-new CPU independently, then integrate the CPU into the on-site control system.

Control Expert manual capture

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: