Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum distance between the HDPM6000 Head Unit and the Last Busway?

Issue

What is the distance limitation from the HDPM6000 Head Unit and last HDPM6000B?

Product Line

HDPM6000B

Environment

HDPM6000 Head Unit and the modules, HDPM6000B Busway limitations.

Cause

There is a distance limitation from the HDPM6000 Head Unit to the last HDPM6000B Busway module

Resolution

  • PowerLogic HDPM6000B Installation Guide (See the HDPM6000 Bus Connection Section): https://www.se.com/us/en/download/document/Z208131/
  • In daisy chain format, the maximum distance between the HDPM6000 head unit and the first module on the CAT6 daisy is <30 m (98 ft.). See Figure 1.

Figure 1. Bus topology for 14 or fewer modules and bus cable length less than 100 feet

Bus topology for 14 or fewer modules and bus cable length less than 100 feet

  • Maximum up to 14 devices can be installed in a daisy chain.
  • If more than 14 modules are connected on one HDPM6000 bus or the total bus cable length exceeds 30 meters (98 ft.), the bus cable must be installed in a ring. See Figure 2.
    • Note:  In a ring configuration, the cable length between the head unit and the last module (through module 1, 2, etc., not including the cable from the last module back to the head unit) should not exceed 51.2 m (168 ft.).

Figure 2. Bus topology for more than 14 modules and bus cable length greater than 100 feet

Bus topology for more than 14 modules and bus cable length greater than 100 feet