Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
EcoSet Config System requirements
Here are the requirements for a PC to run EcoSet Config :

1. Windows operating system only (no touch-based OS or mobile devices)

2. Chromium-based browser (Chrome or Edge; no Firefox or Safari)

3. Dedicated GPU (graphics card)

4. Minimum of 16 GB RAM

5. Only one VEGA tab or window open at a time

6. Screen resolution of 1920 × 1080