Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I select switchgears in EcoSet Config?

To create a new switchgear:

  1. Click and open the required switchboard.
  2. To define and select a switchgear, select the product range from the catalog

(A) and add it to your electrical network. Choose one of the following options:

Note: One of the predefined switchgears can also be made as favorite. In this way, while selecting the product range from the catalogue - the pre-selected switchgear will come as a first solution to add.

    • Select Schneider Pre-configured parameters to define and select a switchgear.
    • Set up customized product specifications:
      • Select the parameters to get the switchgear.
      • Click to save defined parameters with a specific name. You can choose this pre-defined switchgear, as and when required.
  1. Enter the desired quantity and click one of the options below:
    • Add and Continue: To add more products to switchboards.
    • Add: To add the selected products.

Select a Switchgear
Switch gear

Schneider Electric Egypt and North East Africa