Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I select the enclosure in EcoSet Config?

The DESIGN A SWITCHBOARD tab displays the compatible enclosure ranges based on the required space to mount the devices configured previously. You can find module information in the DEVICES TO MOUNT section. To refine your search, update the following sections:

  • SPARE SPACE : Select the modular reserve as per your requirements.
  • GENERAL CHARACTERISTICSOFTHE ENCLOSURE: Select the general

characteristics of the enclosure based on your requirements.

  1. Select the enclosure from Select your range section and click Next.

NOTE: You can only select enclosures which are compatible. Enclosure marked with an orange notification warning icon are not compatible with the type of modules to be mounted.

  1. On the next page, select the detailed characteristics of the enclosure and click

Next.

Select the Enclosure

Image