Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to diagnose line break for BMXART0814/0414 at mV ranges ?

Issue

How to diagnose line break for BMXART0814/0414 at mV ranges ?

Product Line

X80

Environment

Control Expert

Resolution

BMXART0814/0414 modules have the interface to enable/disable the broken wire detection function for thermocouple or thermoprobe signals as below .

TC

User is able to monitor the broken wire through channel and module Error lights at mv range.  Module variables listed below could be used to indicate wire broken status in PLC application .

I/O data type : Device DDT

When the channel selected to +/- mV , CH_HEALTH in Device DDT will report error in case of broken wire.

DDT

I/O data type : Topological

Variables CH_ERROR, CH_FLT, SENSOR_FLT in IODDT could indicate the broken wire error and function block READ_STS could be implemented to read above exact channel status.

IODDT

Schneider Electric Egypt and North East Africa

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: