How can we help you today?

Alternatives to Play a Video in Machine SCADA Expert v2023

Issue:

This FAQ covers the alternatives available in Machine SCADA Expert v2023 to play a video.

Product:

EcoStruxure Machine SCADA Expert v2020, v2023

Environment:

HMI Configuration Software in Windows

Resolution:

To embed and play videos on a project screen in EcoStruxure Machine SCADA Expert, you have two main options:

1- ActiveX / .NET Controls

You can use native objects such as:

  • Web Browser
  • Windows Media Player
  • Or third-party objects like VNC.

Note: ActiveX controls are still supported in Machine SCADA Expert; however, we do not recommend using them anymore since modern alternatives like .NET controls or Custom Widgets are available.

2- Custom Widgets

In a Custom Widget, you can take advantage of HTML5 native compatibility to play videos, create video controls, or fully customize video playback.

ActiveX controls are still compatible with EMSE; however, we no longer recommend using them since modern options like .NET controls or Custom Widgets are available.

Additionally, if the project needs to be accessible to clients, Custom Widgets are the best option, as they make the object available on any web browser and platform through Mobile Access.

The Custom Widget Framework is required to execute Custom Widgets.

You can find the installation package here:

C:\Program Files (x86)\Schneider Electric\EcoStruxure Machine SCADA Expert 2023\Redist\CustomWidgetFramework

Modify video Settings:

1

If you need to hide video controls, proceed as follows:

2

When hovering the mouse over the video, no video controls appear:

3

Import the Widget:

You can copy the widget folder and reuse it in any project:

4

You can also use the .zip file included in this FAQ. Rename it to .cwp and copy it to the folder below:

C:\Program Files (x86)\Schneider Electric\EcoStruxure Machine SCADA Expert 2023\Redist\CustomWidgetsLibrary

5

Before opening it, adjust the width and height:

6

Schneider Electric Egypt and North East Africa

Attachment(s)
CWVideoPlayer.zip [1.17 KB]