Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to access a Bit in a WORD variable in EcoStruxure Operator Terminal Expert?

Issue:

Alternative to access directly a bit of a WORD, without creating a BOOL type variable pointing to this specific bit.

Product:

EcoStruxure Operator Terminal Expert v3.x , v4.x (EOTE)

Environment:

HMI Configuration Software in Windows

Resolution:

Option 1: Define a BOOL variable that points to a specific bit of a WORD.

1

Note: This requires creating a new variable for each bit you need.

Option 2: Use a custom script to automatically create multiple variables. If adapted, the same script can be reused for several variables.

Part of the script:

2

Result:

3

Attached Resources:

  • EOTE Project: Minimum version v3.5 required to open.
  • Control Expert Project: Minimum version v15.1 required.
  • Video: Demonstrates the final result.

Schneider Electric Egypt and North East Africa

Attachment(s)
FAQ000279923.zip [18.02 MB]