How can we help you today?

Are There Any Limitations for the OPC UA Server in EcoStruxure Operator Terminal Expert?

Issue:

Is there any limitation for the OPC UA Server with Operator Terminal Expert?

Product:

EcoStruxure Operator Terminal Expert v3.x , v4.x (EOTE)

Environment:

HMI Configuration Software in Windows

Resolution:

There is no strict limit; however, monitoring a large number of variables can impact HMI performance.

The recommendation from R&D is to keep OPC UA communication variables below 5,000 (this number was validated by R&D in previous tests).

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center