Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum number of lines allowed in a Ladder Diagram (LD) section in EcoStruxure™ Control Expert?

1. Issue

Users need to know the size limitation for Ladder Diagram sections to avoid performance issues and ensure proper project design.

2. Product Line

  • Software: EcoStruxure™ Control Expert
  • Language: Ladder Diagram (LD)
  • Standard: IEC 61131-6

3. Environment

  • Windows OS (e.g., Windows 10/11)
  • Control Expert project with LD sections assigned to tasks (MAST, FAST, AUX).

4. Resolution

  • Limit: Each Ladder Diagram section can contain up to 1000 lines.
  • Best Practices:
    • Use smaller sections for easier maintenance and better performance during online modifications.
    • Apply conditional execution bits to optimize scan time.
    • Assign each section to only one task.