Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I implement a 4–20 mA analog input signal using the TM221CE16T PLC?

Issue:

Is the TM221CE16T PLC capable of supporting a 4–20 mA analog input signal?

Product Line:

M221

Environment:

EcoStruxure Machine Expert

Resolution:

While the integrated inputs on the TM221CE16T are voltage-only, the system is expandable. You can add TM3 I/O modules for current inputs as shown on page 14 of the catalog.

https://www.se.com/us/en/download/document/DIA3ED2140109EN/

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: