Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I migrate the OFS DA configuration file into the Modicon Communication Server OPCUA for AVEVA System Platform?

Issue:

Migrating the OFS DA configuration file into the Modicon Communication Server(OPCUA) for AVEVA System Platform?


Product Line:

Modicon Communication Server, AVEVA System Platform


Resolution:

You can use the Modicon Communication Server to migrate the configuration of OFS DA to OPC UA devices using the data defined in the configuration file (DeviceConfig.xml) for AVEVA System Platform

Follow these steps to migrate from OFS DA to OPC UA

image1

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: