Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Battery Compartment Screw Type for SEPAM 80 Protection Relay

Article available in these languages: Spanish

Issue

Users need to identify the correct tool type and size required to open the battery compartment on the SEPAM 80 protection relay.

Product

SEPAM 80 Protection Relay

Environment

  • SEPAM 80 relay front panel
  • Battery compartment maintenance or battery replacement procedures

Cause

Misidentification of the screw head type on the SEPAM 80 battery compartment, leading to the incorrect assumptions.

Resolution

The battery compartment on the SEPAM 80 relay requires a TORX T08 driver to remove or fasten the screw properly. Using the correct TORX T08 tool ensures safe access to the battery compartment without damaging the screw head or the relay enclosure.