Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the Profibus Remote Master (TCSEGPA23F14F) compatible with the BMXNOC0401 ?

Issue

Is the Profibus Remote Master (TCSEGPA23F14F) compatible with the BMXNOC0401 ?

Product Line

M340

Environment

Control Expert

Resolution

The PRM is supported only by the M340 BMXNOE01x0, not by the BMXNOC0401 .



Schneider Electric Egypt and North East Africa

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: