Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I connect to the Edge I/O Network Interface Module via USB connection

Issue:

USB connection to the Edge I/O NIM


Product Line:

Edge I/O


Resolution:

The USB Port connection is suitable for short-duration connections for the express purposes of configuration, maintenance, and troubleshooting. It is not intended as a long-standing connection for other purposes. Further, the network interface module may only be connected to a PC.

Note: The communication cable should be connected to the PC first to help minimize the possibility of electrostatic discharge affecting the network interface module

image1

To connect the network interface module to the PC, do the following:

image2

You must configure a virtual Ethernet Link on your USB port, before you can access the network interface module through USB.

To configure a virtual Ethernet Link, configure an Ethernet interface of the USB-RNDIS by following the steps below:

image3

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: