How can we help you today?

Smart UPS - 'Mains input bad' Event Messages after switching 3‑Phase input Source

Issue

The UPS logs the following events:

  • UPS: Main input bad. (0x01B0)
  • UPS: Main input bad cleared. (0x01B1)
  • UPS: Main input bad. (0x01B0)
  • UPS: Main input bad cleared. (0x01B1)
  • UPS: On battery power due to frequency and phase difference. (0x010)

These events typically occur when switching from a 3‑phase primary input source to a 3‑phase secondary source, such as a generator, or when switching back from the secondary source to the primary.

Both sources are accepted by the UPS when it is started on either one individually, and no issues occur when the input is changed to single‑phase.

Product Line

SRT8KRMXLI, SRT10KRMXLI

Environment

3 phase input with a secondary source

Resolution

This issue can arise when the phase order is different between the two input sources. At the start-up, the UPS will accept any phase sequence. But during the switchover, it's looking for the same sequence as previously receiving.

two sources showing incorrect and correct phase order

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center