How can we help you today?

HMIST6500, Operator Terminal Expert - Time limit for the clock setting.

Issue:

Why is there a limit for the clock setting. This means that passed Jan 18-2038 the clock will stop functioning?

Time limit on key entry.

Product Line:

EcoStruxure Operator Terminal Expert (all versions), All Harmony, non Windows HMI.

Resolution:

In the EcoStruxure Operator Terminal Expert help, we can fins the below information in regards to the maximum limit on the date and time.

Help section about the time limit.

This is related to the Year 2038 problem. See below the Wikipedia link on this subject for more information.

https://en.wikipedia.org/wiki/Year_2038_problem

R&D provided the more specific information in regards to this problem and a potential workaround:

The 2038 is the maximum value of UNIX time.

If this value is exceeded, an overflow will occur, causing the time to stop or the value to reset to 0 and return to 1901,

which could cause the system to malfunction.

Basically no workaround, by 2038 the development team will usually plan to change, design the software to support 2038 and beyond (e.g. support to 64 bit).

For now, there is no plan for this requirement.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center