How to Power cycle an InRow Cooling Unit Gen2?
PUBLIC
Issue:
How to Power cycle an InRow Cooling Unit Gen2?
Product Line:
InRow Family Gen2.
Environment:
ACRD3XX, ACRC3XX, ACRH3XX, ACRD6XX, ACRC6XX, UNIFLAIR SP, etc.
Cause:
General aid for Customers
Resolution:
- Please click on the home icon (Fig 1) 👇🏻
Figure 1
- Click on the On/Off button (Fig 2), you might be required to input the pin, use the default one: 1234.
Figure 2
- Change the state from on to off (Or StandBy), then click OK (Fig 3).
Figure 3
- When the fans start ramping down, please unplug the dedicated power cord(s) to the unit (It can be top or bottom fed) [Figure 4] or put down the dedicated breaker(s) to the unit (If it’s hard-wired), or if it’s a 600mm InRow (Figure 5) and leave the unit without any power for at least 5 minutes.
Figure 4 (For 300mm InRow only).
Figure 5 (For 600mm InRow only).
- After the 5 min passes, restore the power to the unit, allow a couple of minutes, for the display to pop up, change the mode from Off to On (Figure 3), and test the proper operation of the unit.
NOTE: This process can only be executed from the front display of the unit.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.