Why am I getting a .NET framework 3.5 service pack 1 error during installation of Control Expert 16.2?
Issue:
Why am I getting a .NET framework 3.5 service pack 1 error during installation of Control Expert 16.2?
Product Line:
Control Expert
Resolution:
First make sure the .NET framework is installed and active on your machine
Method 1 — Check via Windows Features
- Press Windows Key + R
- Type:
- Optional features
- Press Enter
- In the Windows Features window, look for:
- “.NET Framework 3.5 (includes .NET 2.0 and 3.0)”
- Status meanings:
- Checked → Installed
- Unchecked → Not installed
- Filled box → Partially installed
Method 2- Check using Command Prompt
-
Open Command Prompt
-
Run this command:
BAT
If .NET 3.5 is installed, you will see a Version entry like:
Version REG_SZ 3.5.30729
Method 3- PowerShell Command
Open PowerShell and run:
Look for:
- Installed → It’s on your system
- Available → Not installed, but can be enabled
Method 4- Check the File System
Look for this folder:
C:\Windows\Microsoft.NET\Framework\v3.5\
If the folder exists → .NET 3.5 is installed.
If it is not installed please go to the windows site here:
https://www.microsoft.com/en-ca/download/details.aspx?id=25150
If it is unchecked, please check it. It might ask permission to update and download new files to complete the installation. Please allow it
After it is done, reboot and check the feature again.
Now you should be able to install the software with no further issues
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.