How can we help you today?

After upgrading to NetBotz 5.5 firmware, clips are no longer attached to e-mail alerts.

Issue:
After upgrading to NetBotz 5.5 firmware, clips are no longer attached to e-mail alerts.

Product Line:
NetBotz

Environment:
NBRK0750
NBWL0755
Botzware 5.5.0

Cause:
After upgrading to 5.5 some customers are experiencing an issue where e-mails are no longer sent.

Resolution:
This issue will be resolved in the 5.6 release but in the meantime, there is a workaround.

Go to the NetBotz top menu and choose Settings-->System-->E-mail
Regardless of "Connection Security" settings, make sure a user name is input into the "Authentications Settings" Username field.

User Name Field

This appears to resolve the issue based on the 5.5.0 upgrade.

Schneider Electric Egypt and North East Africa