Why using GeoScada 2025 with OFS 3.63 SP3 when a write command on a string is sent to the PLC, this one receives only the first character and display on GeoScada only the first character?
From GeoScada when you are sending a write command on a string to the PLC through OFS, GeoScada converts the String into a canonical data type where each character is coded on two bytes (VT-Array): UTF-16)
OFS doesn’t support this conversion in VT_UI2.
However, OFS can expose a proper string as VT-BSTR. To do it, in GeoScada the argument must be added ;C at the end of each item.
It must be done as follows:
The result is the following:
Product line :
GeoScada Version 2025 (Build 87.9397) and above
OFS 3.63 SP3
Released for: Schneider Electric Egypt and North East Africa
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
Help Center
Find support resources for all your needs, in one place.