How do I perform the initial internal battery connection? | Back UPS PRO RS/NS M2, MS & Gaming UPS (BGM series)
Issue:
The Back UPS PRO RS/NS M2, MS & Gaming UPS (BGM series) does not power on or begin charging when first connected.
Product Line:
Back UPS PRO RS/NS M2, MS & Gaming UPS (BGM series)
Environment
BR1000MS, BN1100M2, BR1350MS, BN1350M2, BN1375M2, BN1500M2, BR1500MS, BGM2200-MSX / All serial
Cause:
When purchasing a UPS from the Back UPS PRO RS/NS M2 ,MS & Gaming UPS (BGM) family, it is necessary to perform the initial connection of the internal battery before operating the unit. If this step is skipped, the UPS will not function properly or begin charging its batteries.
Resolution:
See the procedures:
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.