How can we help you today?

Is Cascade function available for the ATS490?

Issue:

Does the ATS490 support the Cascade function?

Product Line:

ATS490

Environment:

Multiple motors

Resolution:

The ATS490 does not include a Cascade start function; for this type of application, we recommend using the ATS480 series.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center