EROE Web Server is Not Reachable Over WAN Network – SCADAPack 474i Routing Table configuration
Symptoms seen: Can't connect to EROE webserver from outside local RTU subnet.
EROE Web server not connecting:
Example Network Topology:
Local Connection:
Even though the EROE Web Server PC and the remote device could communicate locally, see Local Connection, remote access failed because the SCADAPack 474i routing table was not configured to return traffic back to the PC network (10.10.10.0/24) as seen in the Example Network Topology.
This caused one‑way communication, which is why:
- The EROE Web Server PC (10.10.10.224) could send packets toward the remote network (192.168.1.x).
- But the SCADAPack 474i or End Device had no route telling it how to return packets back to the 10.10.10.x network.
- As a result, the web server appeared reachable locally but never responded to network clients, making the web interface inaccessible from the remote side.
Resolution
- Add a NETWORK route in the SCADAPack 474i routing table.
- In RemoteConnect, Configuration → IP Communication → Routing Table
- Add IP Route.
After adding this route, the SCADAPack will know how to return traffic to the PC, and the EROE Web Server will be fully accessible across the network.
For additional information, you can connect to the SCADAPack 474i RTU using Telnet and run the command route print to review the routing configuration on the device. Verify the Edge routing entries to confirm that the required networks and gateway paths are correctly defined.
/user>route print
Interface List:
10: ETHERNET 1 IP Address: 192.168.1.110/27
11: ETHERNET 2 IP Address: 172.16.1.200/24
EDGE(ETH3) IP Address: 172.16.1.201/24
EDGE(ETH4) IP Address: 0.0.0.0
13: USB IP Address: 10.2.3.4/29
RTU Routes:
Type Destination-IP Net-mask Gateway-IP Interface Metric
DFLT-GW 0.0.0.0 0.0.0.0 192.168.1.97 10 0
NETWORK 10.2.3.0 255.255.255.248 10.2.3.4 13 0
HOST 10.2.3.4 255.255.255.255 10.2.3.4 13 0
GATEWAY 10.10.10.0 255.255.255.0 172.20.30.97 10 1
HOST 127.0.0.1 255.255.255.255 127.0.0.1 0 0
NETWORK 169.254.254.248 255.255.255.248 169.254.254.249 11 0
HOST 169.254.254.249 255.255.255.255 169.254.254.249 11 0
NETWORK 172.16.1.0 255.255.255.0 172.16.1.200 11 0
HOST 172.16.1.200 255.255.255.255 172.16.1.200 11 0
NETWORK 192.168.1.96 255.255.255.224 192.168.1.110 10 0
HOST 192.168.1.110 255.255.255.255 192.168.1.110 10 0
Route Priority: HOST NETWORK GATEWAY DEFAULT-GW
Edge Routes:
Type Destination-IP Net-mask Gateway-IP Interface
DFLT-GW 0.0.0.0 0.0.0.0 172.16.1.1 ETH3
NETWORK 10.2.3.0 255.255.255.248 169.254.254.249 EDGE
NETWORK 192.168.1.96 255.255.255.224 169.254.254.249 EDGE
NETWORK 10.10.10.0 255.255.255.0 169.254.254.249 EDGE
RTU NAT Redirections:
Destination-IP Port Redirect-IP Port Protocol
10.2.3.4 22 169.254.254.250 22 tcp
10.2.3.4 443 169.254.254.250 443 tcp
10.2.3.4 4323 169.254.254.250 4323 tcp
192.168.1.110 22 169.254.254.250 22 tcp
192.168.1.110 443 169.254.254.250 443 tcp
192.168.1.110 4323 169.254.254.250 4323 tcp
172.16.1.200 22 169.254.254.250 22 tcp
172.16.1.200 443 169.254.254.250 443 tcp
172.16.1.200 4323 169.254.254.250 4323 tcp
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.