Troubleshooting SmartConnect-compatible UPS Connection to the Cloud
Issue 1: Troubleshooting the UPS Connection to the Cloud
- If you are having difficulty connecting your UPS to Schneider Electric cloud services, see Network Requirements.
- See Issue 2: APC Smart-UPS Device Types below to troubleshoot the connection of your APC Smart-UPS device.
Issue 2: APC Smart-UPS Device Types
There are three device types that can connect to Schneider Electric cloud services:
1. UPS with a Character Display
- Navigate to the Status menu.
- Navigate to SmartConnect:
Issue 3: UPS Connection Status Indicators
| UPS Character Display | UPS Icon Display | UPS Status Indicator | Description |
| No Ethernet | Sc.0 | Indicator not illuminated | The LED indicators above the Ethernet port are not illuminated. Action - Check that the Ethernet cable is firmly inserted into the Ethernet port by disconnecting it and reconnecting it. Once connected, the Ethernet port LED will illuminate. |
| Addressing | Sc.2 | N/A | The device is obtaining an IP address on the local network via DHCP. Action - If this is displayed for more than 2 minutes, check that the configuration of the DHCP server will allow the MAC address of the device. See Network Requirements. |
| Contacting | Sc.4 | N/A | The device is establishing a connection to Schneider Electric cloud services. Action - If this is displayed for more than 2 minutes:
|
| Securing | Sc.5 | N/A | The UPS is securing the TLS network connection. Action - If this is displayed for more than 2 minutes, ensure that the following cipher suites are not blocked in your firewall configuration: TLS_PSK_WITH_AES_128_CCM_8 TLS_PSK_WITH_AES_128_CBC_SHA256 TLS_PSK_WITH_AES_128_CBC_SHA If the above cipher suites are allowed and this status persists, contact APC Customer Support. |
| Connecting | Sc.6 | N/A | The UPS is establishing communication with Schneider Electric cloud services. Action - If this is displayed for more than 2 minutes, contact APC Customer Support. |
| Connected | Sc.1 | Green | The device has established a connection to Schneider Electric cloud services, and is operating normally. |
| Disabled | Sc.7 | Red | Action - Contact APC Customer Support. |
| Prohibited | Sc.8 | N/A | Ethernet connection is not allowed due to a hardware issue or configuration. Contact APC Customer Support. |
Issue 4: Restart the UPS Network Interface
| UPS models with the prefix SMT/SMX/SMTL To reset the network interface of an SMT/SMX/SMTL model UPS, on the display interface hold the UP and DOWN buttons simultaneously for 5 seconds. The display flashes to indicate that the network interface has restarted. | |
| UPS models with the prefix SMC To reset the network interface of an SMC model UPS, on the display interface hold the MUTE and MENU buttons simultaneously for 5 seconds. The display flashes to indicate that the network interface has restarted. | |
| UPS models with the prefix SCL To reset the network interface of an SCL model UPS, insert a paperclip into the Reset pinhole on the rear of the UPS. | |
| UPS models with the prefix SRTL To reset the network interface of an SRTL model UPS, on the touch screen interface navigate to Configuration > Communication > Smart Connect Restart > select Yes. |
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.