PME - How to move Designer modules into or out of a Grouping Object
Issue
There is a need to move modules onto different windows or pages of the same diagram to organize them.
Product Line
ION Enterprise 5.x
ION Enterprise 6.x
StruxureWare Power Monitoring 7.x
Power Monitoring Expert 7.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024
Environment
Designer
Resolution
Note: These steps are for moving modules within the same Designer node (ION meter or VIP). When copying modules to a different node, review the paste window carefully since a lock paste can unintentionally overwrite existing modules.
1. Select the modules you want to move, then open Edit > Copy:
2. Navigate to the other window of the same Designer node, then open Edit > Paste.
3. Lock paste all modules and select Maintain external inputs. To lock paste all modules, select the first checkbox in the list, press and hold the Shift key, then click the last checkbox in the list.
4. Click OK. Changes are automatically saved.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.