How can we help you today?

PME - How to open and save changes to a native device type in Device Type Editor

Product Line

Power Monitoring Expert 9.0

Power Monitoring Expert 2020

Power Monitoring Expert 2021

Power Monitoring Expert 2022

Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment

Device Type Editor

Resolution

Note: If there are PME driver files (.ion and .xml) with the same name in both of these folders below, PME will always use the version of those files located in the …\config\translators folder.

  • …\Program Files (x86)\Schneider Electric\Power Monitoring Expert\system\translators
  • …\Program Files (x86)\Schneider Electric\Power Monitoring Expert\config\translators

1. Open File Explorer, then navigate to …\Program Files (x86)\Schneider Electric\Power Monitoring Expert\system\translators.

2. Copy the .ion and .xml file for the device type you want to edit.

3. In File Explorer, navigate to …\Program Files (x86)\Schneider Electric\Power Monitoring Expert\config\translators.

4. Paste the .ion and .xml files into this folder.

5. Open Management Console > Tools > System > Device Type Editor:

Device Type Editor

6. File > Open, then navigate to …\Power Monitoring Expert\config\translators:

config translators folder

7. Open the previously copied .ion file.

8. Make the desired changes, which can include changes to software logging.

9. File > Save.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center