How can we help you today?

NetBotz 250A supports multiple rope leak sensors with firmware 3.3.x or newer.

Issue:
NetBotz 250A supports multiple rope leak sensors with firmware 3.3.x or newer.

Product Line:
NetBotz

Environment:
NBRK0250A
Firmware version 3.3 or higher.

Cause:
Initial NetBotz 250A firmware did not support leak rope sensors.

Resolution:
As of firmware version 3.3.1.1 AOS and 3.3.0.2 250A application, the NetBotz 250A now supports multiple leak rope sensors connected to the universal sensor ports.

Please note that EcoStruxure IT Data Center Expert may not see the new leak rope sensors properly without the attached APC environmental DDF.

Schneider Electric Egypt and North East Africa

Attachment(s)
apcenv v27.zip [5.08 KB]