How can we help you today?

How to perform self-test on Back-UPS products?

Issue: Understanding the operation of the Back‑UPS self‑test and what happens during the test.

Product Line: Back‑UPS/Back-UPS Pro products

Cause: Users may need to test the battery inside the UPS to check battery condition.

Resolution:

By default, Back‑UPS units automatically perform a self‑test each time they are powered on to check battery condition and estimate runtime. During the self‑test, the UPS briefly switches to battery power for about 10 seconds, then returns to normal AC operation. For accurate results, the connected load should be between 10% and 30% of the UPS’s rated capacity, as lighter or heavier loads may lead to inaccurate runtime estimates.

For more details, see Back‑UPS Basic Self‑Test Theory Explained.

DISCLAIMER: If the self‑test is performed incorrectly or if unsupported methods are used, there is a risk of dropping the connected load.

There are two self‑test methods that can be performed while the UPS is powered on without dropping the load:

1. Manual Self-Test

Make sure the Back‑UPS is plugged into a power source and turned on. Press and hold the power button. Keep holding the button until you hear two beeps or see the online LED start blinking, then release the button. This starts the manual self‑test.

Front panel of a Back‑UPS Pro showing the power button highlighted. A red box and arrow indicate pressing and holding the power button to start the self‑test. LCD display showing the self‑test in progress. An arrow points to the screen where the UPS has switched to battery mode and is running diagnostics LCD display showing ONLINE status. The screen indicates the test has completed, and passed it self-test.

Front view of an APC Back‑UPS BVN900M1 with a red box and arrow highlighting the power button.Front panel of APC Easy UPS BX 700VA, 1000VA, 1400VA, 1500VA. Highlighting the ON/OFF button.

2. PowerChute Serial Shutdown (PCSS)

This method uses software. Use this option if your Back‑UPS is connected to a computer that has PowerChute Serial Shutdown (PCSS) software installed.
a. Open a web browser on the computer connected to the UPS and log in to PowerChute Serial Shutdown.
PowerChute Serial Shutdown (PCSS) Login Screen
b. Click the UPS Model Name, then select Diagnostics.
Screenshot showing where to locate the Diagnostics page.
c. On the Diagnostics page, locate Initiate Diagnostics. From the select diagnostic action drop‑down menu, select Self Test.
Screenshot showing how to select Self Test from diagnostic action dropdown menu.
d. Click Apply to start the self‑test.Click Apply Button
e. Monitor the Self‑Test Status and confirm whether the result shows Passed, or Failed.
Screenshot showing Self Test In Progress
Screenshot showing Self Test Passed

Note: Self‑test procedures may vary by UPS model. Always refer to the applicable UPS user manual guide for specific instructions.
If you have any clarifications, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center