How can we help you today?

Power Monitoring Expert (PME) How to capture OPC UA Logs

Issue
Power Monitoring Expert (PME) can function as an OPC UA server and/or client. OPC UA logs can be used for analysis.

Product line

Power Monitoring Expert 2024

Environment
Power Monitoring Expert (PME)

Cause

See here for configuring PME as an OPC UA client and here as a server. OPC UA logs can aid in resolving issues that may occur.

Resolution

  1. Navigate to the [PME installation folder]\system\bin  (Typically found at C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\system\bin)
  2. Open the OpcUAserver.exe.config
  3. Enable the opc logs, by changing the text below from "false" to "true"
    C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\system\bin\OpcUAserver.exe.config file entries "logenabled" and "realtimelogenabled"
  4. Restart the OPC UA Windows Server service
  5. A log folder shall be created under %programdata%/schneiderelectric/PME/OPC/server/
  6. Note: Do not keep these logs enabled for too long; recommended only while the issue is occurring. If these are enabled for longer, this may consume system space, and if not turned off it may slow down the system.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center