What is the cause of the FWPF error on an ATS480?
Issue:
What are the possible causes of an FWPF error on an ATS480?
Product Line:
ATS480
Environment:
Display shown on the VW3A1111 keypad
Resolution:
If the ATS480 is powered on with the VW3A1111 keypad and it displays a FWPF fault, with the soft starter powered off, remove the VW3A1111 keypad and connect the mini keypad that comes with the unit. Then power it back on and press OK to clear the fault.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.