Why do I see a Runtime Manager trial pop-up after activating my Vijeo Designer Runtime v6.2 SP12 license?
Issue
On every HMIP6 startup, the Vijeo Designer Runtime Manager launches automatically and shows:
"Welcome to Vijeo Designer Trial Edition"
This occurs even though the Runtime license is already activated.
Product Line
HMIP6 family
Environment
Vijeo Designer Runtime v6.2 SP12
Cause
The Runtime Manager belongs to a legacy licensing system.
Vijeo Designer Runtime v6.2 SP12 uses the License Manager that does not rely on Runtime Manager.
As a result:
Runtime Manager may still start automatically
It may incorrectly display a Trial Edition message
This message does not reflect the actual license state
Resolution
If the license is valid and Vijeo Designer Runtime starts without licensing errors, the message can be ignored.
To prevent this pop up from showing, follow these steps:
1. Confirm license activation
-Open License Manager
-Verify the license status shows Active
2. Validate Vijeo Designer Runtime operation
-Launch Vijeo Designer Runtime
-Confirm no license-related errors appear
3. Disable the pop up
-Locate Runtime Manager executable under:
C:\Program Files (x86)\Schneider Electric\Vijeo-Designer 6.2\Vijeo-Runtime\Public\Bin
-Run Runtime Manager as Administrator by right clicking the RuntimeManager.exe and select Run as Administrator
-Check: "Do not display this dialog again"
-Click Exit
After this, the trial message will no longer appear during startup.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.