How can we help you today?

UL Certification of MiCOM P99x Test Blocks

Article available in these languages:

  • Spanish

Issue

Clarification is required regarding whether MiCOM P99x Test Blocks are UL certified.

Product

MiCOM P99x Test Blocks

Environment

All installations and applications where UL compliance or certification verification is required.

Cause

Users may not find clear or readily available documentation confirming the UL certification status of MiCOM P99x Test Blocks, leading to uncertainty during compliance checks or project approvals.

Resolution

MiCOM P99x Test Blocks are UL certified and are officially Listed under UL file number E155724.

To verify certification:

  • Refer to UL documentation using file number E155724
  • Confirm listing through UL databases or Schneider Electric product documentation

This certification ensures that the product meets applicable UL safety standards and can be used in installations requiring UL-listed components.

Schneider Electric Egypt and North East Africa
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
  • Help and Contact Center