Video: How to solve the READ_NUA_DDT Function Block that stops updating the BMENUA0100 status variable after a swap over from Primary to Standby on a M580 redundant system
Issue :
The READ_NUA_DDT function block stops updating the value of the T_BMENUA0100 variable in a M580 hot standby/redundant system when swapping the Primary and Standby role of the 2 CPUs.
Product Line :
Control Expert
M580 hotstandby
BMENUA0100
Cause :
This is caused by the fact that the data of the management table of the READ_DDT block found inside the READ_NUA_DDT dfb is part of the data that is exchanged between both CPU. This might cause this block to stop operating when a swap occurs. It is explained in the help file of the block
Resolution :
To fix this, we need to disable the Exchange on STBY option for the instances of the READ_NUA_DDT blocks like shown below :
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.