What is the right method to handle the unused power cables on SNAP IN Busbar?
The power cables (flexible wires) on SNAP IN busbar are used to distribute the power from busbar to GV2(snap in version). They are fixed in the safety hole when delivery to customer.
- When select the SNAP IN busbar, please choose the proper busbar commercial reference whose number of tap-offs equals to number of GV2 which will be installed under the busbar, in this case, there won’t be unused power cable to be handled.
- In case number of GV2 is less than the number of tap-offs from busbar, please follow the Instruction sheet NAT1303101 to always keep all unused power cables inside the safety hole with the grey mark covered up, failure to follow these instructions can result in death, serious injury, or equipment damage.
One example:
There is one grey mark on the surface of the cable in image001 in red highlighted.
image001
image002 is not OK because the grey marks on the surface of the wires are visible. Customer should push the cable more inside the holes.
image002
image003 is OK because the grey marks on the surface of the wire are inside the holes.
image003
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.