How can we help you today?

TMC4AI2 diagnostic doesn't work with customized range

Analog Input Diagnostics of TMC4AI2 are hard coded in the firmware of the cartrigde.

The diagnostics of the Out of range works correctly with  the default value of inputs range ONLY

0 - 10000 for 0V -> 10V

4000 - 20000 for 4-20mA

Example:

If we use customized input range as 400 - 2000 for 4-20mA, the diagnostics will show an out of range becuse and the range is less than 4000.

(It will be the same for the over range (Out of range diagnostic) if we use a range >20000)

TMC4AI2 Diag

To avoid bad diagnostic bahavior, we have to keep the default value of the inputs range

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center