How can we help you today?

How to Adjust the Session Timeout for PowerChute Serial Shutdown (PCSS)

Product

All versions

Environment

All supported Windows operating systems

All supported Linux operating systems

Issue

A customer wants to modify the session timeout setting for the PCSS web user interface (UI).

Background

Session timeout is an important security and performance feature in web applications. It helps PCSS users to:

  • Prevent unauthorized access if a session is left unattended
  • Reduce the risk of attackers exploiting active sessions
  • Remove idle sessions to improve overall application performance

Default Behavior

By default, the PCSS web UI session timeout is set to 15 minutes.

Resolution:

To adjust the session timeout, stop the PCSS service and then modify the configuration file below:

APC\PowerChute Serial Shutdown\agent\etc\webdefault.xml

Locate the following section:

<!-- ==================================================================== -->

<!-- Default session configuration                                        -->

<!-- ==================================================================== -->

<session-config>   

<session-timeout>15</session-timeout>

</session-config>

Change the Timeout Value

Update the <session-timeout> value to the desired duration (in minutes).

For example:

  • 5 = 5 minutes
  • 60 = 1 hour

After making the changes, start the PowerChute service and check if it has taken effect.

Note: Please be advised that upgrading the software reverts the setting back to the default 15 minutes.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.
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
  • Help and Contact Center