How can we help you today?

Can the Subring assignments on the Predefined config files for the Modicon Extended Managed Switch be changed to DIO Ports?


Product / Platform

· Modicon M580

· Modicon Extended managed Switch


Problem

Customer does not have RIO or DIO Subrings, but would like more DIO Cloud ports on the Modicon Extended Managed Switch using the Predefined files.


Environment

M580 CPU, standalone or HSBY using Modicon Extended Managed Switch


Soluton:

The Predefined file can not be changed.

On page 22 of the Complex Topology guide, it says:


"When you download this DRS predefined configuration file to a switch, the file provides a set of operating parameters that enable the switch to operate with high efficiency in the specified architecture. Except when enabling or disabling ports that are not connected to either a main ring or a sub-ring, do not adjust the configuration parameters or alter the port usage in the predefined configuration file. Changing the configuration parameters or the port assignments can compromise the effectiveness and accuracy of the switch, as well as the performance of the RIO network."


If the customer needs more DIO ports, their options are to use the Service Port of the CPUs or to add an Unmanaged switch to the DIO Cloud ports.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center