How can we help you today?

What are the basic machine requirements for installing the EcoSet Design

System Requirements & Compatibility Guide

To ensure optimal performance and a seamless experience, please review the following system requirements before using the application.

Hardware Requirements

Your system should meet or exceed the following minimum specifications:

Memory (RAM): 8 GB or higher

System Type: 64-bit operating system

Storage: Minimum 500 MB of free disk space

Graphics: Basic graphics card

Recommendation: A modern graphics card with hardware acceleration is advised for enhanced performance and visual quality

Display Resolution: Minimum 1280 × 720 pixels

Supported Operating Systems

This application is compatible with the following Windows versions:

Windows 8

Windows 8.1

Windows 10

Windows 11

Note: We recommend using Windows 10 or later for the best performance and security.

Network Requirements

A reliable internet connection is essential for accessing and using the application effectively.

Network Configuration:

IPv4: Required

IPv6: Optional

Required Open Ports:

To ensure uninterrupted connectivity, please allow access through the following ports:

Port 80 (HTTP)

Port 443 (HTTPS)

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center