How can we help you today?

What is the Programming Software for the Modicon M241?

Issue
Inquiry on the Programming Software for the Modicon M241.


Product Line
EcoStruxure Machine Expert


Environment
Windows 11, Windows 10


Resolution

The software to program the Modicon M241 is EcoStruxure Machine Expert (formerly known as SoMachine).
In order to install this software you need to download "Schneider Electric Software Installer" from the next link:

Schneider Electric Software Installer – Setup

Schneider Electric Software Installer
Then you should be able to install EcoStruxure Machine Expert.
The software EcoStruxure Machine Expert has a Free version after the 42 days trial, please check pages 14 and 16 for more information for the free version limitations:
https://download.schneider-electric.com/files?p_Doc_Ref=DIA3ED2180701EN
Catalog EcoStruxure Machine Expert

The user that wants to use this software needs to have an account in our License Portal in order to register the software:
https://www.se.com/ww/sites/corporate/en/support/software-licensing/user-login

In the past the software was SoMachine and the latest version of this software was the SoMachine V4.3 SP2.
The reference for SoMachine is the SOMNACS43:
https://www.se.com/ww/en/product/SOMNACS43/somachine-software-v4-3-usb-drive-format/

The firmware version of the Modicon M241 for PLC programmed in SoMachine starts in v4.0.x.x., the latest version of the firmware for SoMachine v4.3 is the v4.0.6.41 due to hardware changes.

The firmware version of the Modicon M241 for PLC programmed in EcoStruxure Machine Expert v1.2.x starts in v5.0.x.x.
The firmware version of the Modicon M241 for PLC programmed in EcoStruxure Machine Expert v2.1.x starts in v5.1.x.x.

The firmware version of the Modicon M241 for PLC programmed in EcoStruxure Machine Expert v2.2.x starts in v5.2.x.x.

If you install the EcoStruxure Machine Expert , please select also the installation of the "Controller Assistant" so you can check this information.

In order to program the Modicon M241 you can use a Mini-USB cable (TCSXCNAMUM3P or BMXXCAUSBH018) , an SD Card or an ethernet cable.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center