How do I Activate/Deactivate the EWF (Enhanced write filter) on Windows 7?
Issue
File writes or program installation to the main drive of a Magelis iPC are not being kept before and after a restart because the disk volume is write-protected.
Product Line
Magelis iPC, HMIG5U, HMIG5U2, HMIG5U22, Harmony P6
Environment
Windows 7 Embedded
Cause
The main disk volume of the iPC is write-protected in order to maximize the life of the disk as well as ensuring the saved state of the disk for consistent behavior day-to-day for applications which need it (for example a factory HMI). This is done through a feature called the Enhanced Write Filter in Windows 7 (EWF) and the Unified Write Filter in Windows 10 (UWF)
Resolution
Verifying current state of EWF:
- Click on the** Start** button on your PC.
- Please now select the Run option and at the command prompt type** cmd** (make sure there's administrator rights... if not run as administrator)
- You will now be presented with a black command prompt window and within this will need to type – ewfmgr c:
- This will now return a series of results and will tell you the current state of the EWF.
The Windows Taskbar will also indicate the EWF status:
See the screenshot: "Windows Taskbar EWF State.png"
EWFMGR activate and deactivate commands to use:
To use any of the following commands then you will need to firstly navigate to the command prompt window with the following steps:
- Click on the Start button on your PC.
- Please now select the Run option and at the command prompt type cmd
- You will now be presented with a black command prompt window and begin typing the following commands:
ewfmgr.exe c: -Enable
Activates the EWF from the DOS cmd prompt.
ewfmgr.exe c: -Disable
Deactivates the EWF from the DOS cmd prompt.
ewfmgr.exe c: -commitanddisable
Commits changes that exist in the RAM state to the drive, then deactivates the EWF from the DOS cmd prompt
The Graphical User Interface to Activate/Deactivate EWF can also be used (EWF Windows GUI.PNG):
1. Double-click on the padlock icon and the :Enhanced Write Filter: Overview” popup should appear.
2. Select the “C:” row.
3. Click on “Configure…”
4. Select “Disable”
5. Tick the “Commit” Checkbox
6. Click OK
7. Windows Restart windows from the Start bar.
-
To Activate/Deactivate the UWF (Unified Write Filter) on Windows 10, please see this FAQ: https://www.se.com/us/en/faqs/FAQ000245569/
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.