How can we help you today?

PAS600 Panel Server: Converting old Custom Model format files to the new Custom Model format files

Issue

Older formatted Custom Models cannot be uploaded to the PAS600 with firmware version 2.4.0 and newer.

Product Line

PAS600

Environment

Hardware

Cause

When firmware version 2.4.0 was released, the Custom Model format updated for efficiencies in building Custom Models and customer conveniences.

Resolution

Because the firmware on the PAS600 cannot return to older versions, the only solution is to update the Custom Model files to be accepted on the newer firmwares. On the EPC-W Custom Model Creator Website, old data Custom Model formats can be transformed into new data Custom Model formats.

To begin converting to the new data Custom Model format, go to the EPC-W website, go to the "My Models" page for Custom Models. On this webpage, you can identify "Legacy" or older format Custom Models by finding a white flag icon next to the custom model, in the My Models' list:

EPC Website Old Format

Click on the white flag that corresponds to the custom model file you would like to update and view the Model Compatibility Notice:

Model Compatibility Notice

After viewing the Compatibility Notice, adjust the state of the Legacy/older custom model file to "Limited Release" or "Global Release":

EPC

With the custom model in one of the states mentioned above, create a new version of the Custom Model:

RETAINING DATA NOTE (1/2): In order to keep from losing data within the Panel Server through a firmware update for an existing device, you MUST export and upload the new custom model file with the exact name as the old custom model file.

EPC

Once the new version is created, export it:

EPC

This custom model file can now be uploaded to PAS600's with firmware versions 2.4.0 and newer.

RETAINING DATA NOTE (2/2): If a Legacy (older) Custom Model existed in the Panel Server when uploading the new Custom Model, the new custom model file will be displayed in the "Available Version" column. You must click on the 3 stacked dots icon and switch the Custom Model from LEGACY to NEW to keep all of the data previously stored in the Panel Server.

EPC

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center