How can we help you today?

Video: How do I upgrade the firmware in a Automation Expert M251 dPAC controller?

Issue:

M251 dPAC firmware updating


Product Line:

Ecostruxure Automation Expert, M251


Resolution:

You will need the firmware file for the EAE version you are using. To locate the firmware file, unzip the downloaded EAE zip file.  For example : 25.0.25352.31.zip. When unzipped, you will see the firmware folder. Inside the folder you will see the firmware file for the M251.

image1

Copy this file to the Ecostruxure Automation Device Maintenance utility package location

image2

Select "add"  then select the TM251MDESE from the catalog. Next enter the default IP address of the M251 controller.

The default IP address of an M251 controller can be determined by converting the last 2 octets in the MAC address. The first 2 octets of the IP address is fixed at 10.10. x.y where x.y  is the last two octets of the MAC address

Example:  If the MAC address is 00.00.54.C4.F8.9A. then the IP address will be 10.10.248.154
F8 Hex = 248 Decimal
9A Hex = 154 Decimal

image3

Next enter the login credentials. The default user and password is

User:  installer

Password:  Inst@ller

image4

Next select "update center" and then select firmware

image5

Select desired firmware and select "save"

image6

Next select "Deploy" then "firmware" then "next" .

image7

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center