How can we help you today?

PowerLogic EM3570AX – Current Readings Displayed as 0 A Due to Current Suppression Setting

Issue
A PowerLogic EM3570AX meter displays 0 A on all three current channels after the Rogowski coils are installed.

The meter remains accessible through its embedded webpages, and rebooting the meter does not restore the current readings.

The R-Coil type and 5000 A primary settings appear as read-only and cannot be changed.

Product Line
PowerLogic EM3570AX

Environment
PowerLogic EM3570AX
Rogowski coils
PowerLogic ION Setup
Embedded meter webpages
Current measurement

Cause
The EM3570AX is designed for use with Rogowski coils. The R-Coil type and 5000 A primary settings are fixed and read-only by design.

The Ampere Suppression setting is used to prevent low-level current signals from being displayed. When this setting is configured at 1.0%, relatively low load-current values may be suppressed, causing the meter to display 0 A even though the Rogowski coils and current-input channels are operating correctly.

Resolution
Use PowerLogic ION Setup to reduce the Ampere Suppression setting:

  1. Open PowerLogic ION Setup and connect to the EM3570AX.

  2. Open the meter Setup Assistant.

  3. Open Advanced Setup.

  4. Select Amps Suppression and click Edit.

  5. Change the setting from:

    1.0% -> 0.1%

  6. Click OK, and then click Send to save the change to the meter.

  7. Verify the current measurements using the ION Setup real-time data screens or the embedded webpages.

In the reported case, current measurements appeared on all three phases after changing Ampere Suppression to 0.1%:

  • Ia: 10.043 A
  • Ib: 12.814 A
  • Ic: 7.043 A
  • Average current: 9.967 A

This confirms that the Rogowski coils and all three meter current-input channels are responding correctly.

No firmware upgrade or meter replacement is required when lowering the Ampere Suppression setting restores the expected current measurements.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center