How can we help you today?

RemoteConnect Logic Status Code: -8463 (16#DEF1) Character String Transfer Alert.

What is a Character String Transfer Alert?

A Character String Transfer Alert occurs when a string operation attempts to:

  • Transfer more characters than the destination string can hold.
  • Copy data into a string that exceeds the maximum configured length.
  • Concatenate multiple strings and exceed the destination string capacity.
  • Receive malformed string data from an external device

String1

How to diagnose in Logic Editor (Control Expert).

  • Go to Mode menu and then connect to the device.
  • Go to Tools menu and select Diagnostic Viewer

String2

Examine the Diagnostic Viewer window and it will provide the location of the error in the program.

String3

In this example program, the variable "Result_String" was set to default 16 characters limit which was causing the issue.

Assigned Variables:

String4

Program:

String5

To correct the issue, increase the variable "Result_String" to have a 32 character limit by changing the Type to String[32]

String6

Summary

The RemoteConnect String Overflow Error corresponds to Control Expert's Character String Transfer Alert (-8463 / 16#DEF1). The alert occurs when a string operation attempts to move, copy, or build a string larger than the available destination size. To diagnose the issue, monitor %S15, inspect string handling logic, review communication data received from RemoteConnect, and verify that all PLC string variables are sized appropriately.