How can we help you today?

How to configure automatic variable timestamping on the BMENOP0300 module acting as a server

There are generally three ways to integrate the timestamp corresponding to a Data Object (DO) state change:

  1. Automatic Timestamping

    • The module automatically updates the timestamp value (Data Attribute "t") within the variable.
    • This is only possible when the "t" attribute is not included in the module I/O Mapping.
  2. Manual Timestamping

    • The user manually writes the timestamp value into the Data Attribute "t" through the PLC application and the Device DDT.
    • In this case, the "t" attribute must be included in the module I/O Mapping.
  3. ERT Timestamp Module with SOE Functionality

    • Timestamping can be managed through an ERT timestamp module using the Sequence of Events (SOE) feature.
    • Refer to the product documentation for detailed implementation guidelines.

To enableautomatic timestamping, the Data Attribute "t" must not be mapped in the module I/O Mapping when operating in Server mode. This allows the module to manage and update the timestamp automatically whenever the Data Object changes state.

Consider the Data Object "AlmTOut":

  1. In the I/O Mapping, map only the "stVal" attribute.
  2. Do not map the "t" attribute in the I/O Mapping.
IEDCT screenshot1
3. In the corresponding report dataset, add the "AlmTOut" Data Object and select both the "stVal" and "t" attributes. Including the t attribute in the dataset is required so that the timestamp is published when a report is generated.
4. After inserting the Data Object with both attributes selected, the Attribute column may appear blank. This is normal and expected behavior:

IEDCT Screenshot 3

With this configuration, the module will automatically update the timestamp associated with "AlmTOut" each time its state changes.
IEDScout

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:

Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center